AXIS#.WS.T

Description

This parameter defines the duration for each different current-vector while the coarse angle calculation. The move distance is proportional to the AXIS#.WS.T and AXIS#.WS.IMAX value.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

ms

Range

1 to 200 ms

Default Value

2 ms

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.WS.T

5013h

04h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6707

1

6707 (0x1a33)

AXIS1.WS.T

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.WS.T

6707

Unsigned8

Read/Write

-